(0)| 6/10/2011 1:22 PM | |
|
Posts: 63 Rating:
|
Hello, In below link you will get operaring instruction of MM4 and go commissioning section. For quick commissioning you will not need to adjust the motor data. https://support.automation.siemens.com/WW/llisapi.dll?query=operatin+instruction+of+mm440&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx&lang=en&siteid=cseus&objaction=cssearch&searchinprim=0&nodeid0=4000024&x=0&y=0 |
| 6/10/2011 4:35 PM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
For Temp related issue, I suggest you to perform autotunning.. It is very imp in case you are not having Temp Sensor Please have a look at the attached page of Manual And regarding Speed Response, Which control Mode you are using?? Try Setting Ramp Rounding time to zero.. Regards Devesh AttachmentThermal Model.pdf (297 Downloads) |
Last edited by: Vithani at: 6/10/2011 5:03 PMI dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to
|
|
| 6/10/2011 7:00 PM | |
|
Posts: 6 Rating:
|
I've run the autotuning and the results are the values i wrote in my previous post. With the autotuning the motor weight was automatically set to 32.5 Kgs. Anyway the pdf is very interesting, i'll try to "play" with the other variables such as rotor resistance. Thanks also for the suggestion for the "ramp" rounding, i'll look for this parameter. new question is splitted to Is there any way to set a ratio based on the frequency and change the shown unit?. |
Last edited by: O_Moderator at: 6/14/2011 8:23 AM |
|
| 6/10/2011 7:11 PM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Hey have a look at attached File and try to implement for your case.. It will help you to increase Speed Linearly in the step of 0.1 Hz.. Try and Come back with results.. And regarding your other Qn, yes it is possible...I have to take a look and I will reply you soon with Para Settings.. Regards Devesh Vithani AttachmentVariable RFG for MOP.pdf (297 Downloads) |
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to
|
|
| 6/13/2011 9:21 AM | |
|
Posts: 6 Rating:
|
Vithani, many thanks for all the advices! I'm going to try'em all today, i'll let you know if i'll be able to solve all the issues. Alessandro |
Follow us on