(0)| 6/10/2011 7:00 PM | |
|
Posts: 6 Rating:
|
[schnippschnapp] With another motor i need to display a "m/min" or "m/s" value instead of the rotational speed. Is there any way to set a ratio based on the frequency and change the shown unit? Sorry for the stupid questions, but i've never worked with Siemens vsd... i'm lot more experienced with other brands.
Splitted from M440 - 1st setup advices. |
Last edited by: O_Moderator at: 6/14/2011 8:21 AMnew subject after splitting |
|
| 6/10/2011 7:31 PM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Ok here is solution for your Second Question.. You can use Multiplier.. See attached function Diagram. Set Frequency or RPM in Index 0 and your multiplier Value in Index 2 with the use of P2889/P2890 And set Output of that Multiplier In P0005 and you will get Display whatever you want.. Example: P2800 - 1 P2802.8 - 1 P2877.0 - 21 P2877.1 - 2889 P2889 - 50% P005 - 2878 Now you will get Value on dispay = r021*.5 i.e. Half of the Frequency.. I hope I didnt made this thing complicated Now also have a look at BICO as you are not fully aware with Siemens Drive.. Regards Devesh Vithani AttachmentFn Diagram.pdf (275 Downloads) |
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to
|
|
Follow us on