Hello!
First problem: try changing the system date - i think there is a bug with 29/02...
(1)| 2/29/2012 1:33 PM | |
|
Posts: 6 Rating:
|
Hello, Im using a S7-1214C DC/DC/DC firmware 2.2 with Tia portal v11 sp2. Everything was working fine until today. I download an FC to the plc online and the software says the block was downloaded sucessfuly but its says the blocks are different and I cant monitor the block. Have to do a full upload from the plc! I can confirm that after the download the changes are made in the plc but in the sofware it keeps saying the online block and offline block are different! Tried to go offline and online, tried to load a different project, tried a diferent computer and it allways do this. Anyone got a clue what is happening? I just started doing this today!!!! second question is splitted to Problem with MMC card |
Last edited by: O_Moderator at: 01.03.2012 09:24 |
|
| 2/29/2012 1:43 PM | |
|
Joined: 9/26/2011 Last visit: 9/9/2025 Posts: 5 Rating:
|
Hello!
First problem: try changing the system date - i think there is a bug with 29/02... |
| 3/1/2012 8:54 AM | |
|
Posts: 1 Rating:
|
Also the same for me, I lost 5 hours of trying to figure why I cannot synchronise my blocks. When I changed the date, everything got right. Thank you Siemens. |
Follow us on