1/29/2013 7:20 AM | |
Posts: 48 Rating:
|
Can anybody please tell if we have a instrument having power rating in KVA or KV how can we convert it into kW rating? |
1/29/2013 8:00 AM | |
Joined: 1/8/2008 Last visit: 8/5/2025 Posts: 264 Rating:
|
Hello, P = U x I 1W = 1V x 1A = 1VA = 1W 1kVA = 1000 x VA = 1000 x W = 1kW regards |
1/29/2013 12:39 PM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
S = 1 VA= Apparent Power [VA]= 1V * 1A P = 1 Watt = Active power [Watt] = Apparent power * Cos (Phi) While "Cos (Phi)" = PF "Power factor" Q = 1 VAr = Reactive power [VAr]= Apparent power * Sin (Phi) In most cases (most governments) apply penalities for bad power factor. For avoid these penaities, you have to improve the power factor. AttachmentPFC.pdf (417 Downloads) |
Ayman Elotaify |
|
Follow us on