(0)| 9/9/2013 8:16 AM | |
|
Posts: 19 Rating:
|
Dears All, I am proposing one system.There are two remote stations. Each with S7 400H with ET200M Redundant Bundle & CP 343-1 with Open Modbus/TCP Blocks. These RTU's needs to remotely communicates via Modbus TCP/IP to GSM Gateway with the central SCADA WinCC 7.0 I am using CP 343-1 with Open Modbus/TCP Blocks only for communicating to WinCC SCADAthrough Modbus TCP/IP to GSM Gateway. The Client requirement is to use GSM Network and Modbus TCP/IP. This is relative small system so I am not going on telecontrol system. Both RTU's acts as Server ( Slaves) and WinCC SCADA as Client (Master), which collect data and send commands to RTUs. Can you kindly suggest me , This is a feasible solution & it works. Thanks in advance. AttachmentProposed Configuration.pdf (186 Downloads) |
| 9/9/2013 8:27 AM | |
|
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread RTU's with CP343-1 & Open Modbus TCP , Communicating remotely to WinCC SCADA 7.0 Central Station (Master) Best regards O_Moderator |
Follow us on