(0)| 10/17/2007 12:42 PM | |
|
Posts: 1776 Rating:
|
Hi, check the WinCC diagnostic files on the server and client. How it works see FAQ http://support.automation.siemens.com/WW/view/en/22892165 For compatibility WinCC V5 see FAQ http://support.automation.siemens.com/WW/view/en/21927668 |
| 10/18/2007 11:16 AM | |
|
Posts: 145 Rating:
|
Goodmorning, Well, to avoid further misconception, when I said client's project, I meant the customer's project. The problem exists onlyat the one server. The Runtime freezes permantnently, so the administraotr had to reboot the pc. Best Regards Amateur AttachmentDiagnose.zip (156 Downloads) |
| 10/18/2007 1:30 PM | |
|
Posts: 1275 Rating:
|
Hi, I found the following error in your logs: 2007-09-28 12:54:39,625 ERROR Cannot connect to "MPI_CENTER_CONNECT_1": Errorcode 0xFFDF 42C2! Check these threads out: 1 and 2. Best regards, Danielle |
| 10/18/2007 7:48 PM | |
|
Posts: 1275 Rating:
|
Hi, That's weird.. Best regards, Danielle |
Follow us on