(0)| 10/4/2016 11:53 AM | |
|
Posts: 1 Rating:
|
Hello Experts, I have been trying to install a 2008 SP3 version of WinCC on a Windows 7 32 bit laptop, and the installation proccess always stops when tring to install Microsoft SQP Server 2005. The error message a i receive is "The Following program could not be installed: Miscrosoft SQL Server 2005 Express Edition SP4 setup cannot complete the installation. "107 Unknown MSI Error Code : 107" (below is a screenshot attached ). Has anyone an ideea what could cause this ? how can i fix this ? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/5/2016 1:54:18 PMNew subject after splitting |
|
| 10/5/2016 3:40 PM | |
|
Joined: 7/5/2013 Last visit: 1/16/2026 Posts: 3275 Rating:
|
Hello leomalex, with a search engine and the string "unknown msi error code 107" I found an entry here in the forum: https://support.industry.siemens.com/tf/ww/en/posts/wincc-flexible-2008-install-unknown-msi-error-code-2/26368?page=0&pageSize=10 If this helps, maybe next time you could first search the forum for your issue. Best regards, Frink |
|
Pi is exactly three! |
|
| 10/5/2016 4:00 PM | |
|
Joined: 5/12/2006 Last visit: 1/16/2026 Posts: 22827 Rating:
|
you found this topic because the post was splited from the linked topic and the new topic name was linked. |
| 10/6/2016 9:28 AM | |
|
Joined: 9/3/2008 Last visit: 1/5/2026 Posts: 947 Rating:
|
If you have a newer version of SQL server installed (like SQL 2008), then it may cause the installation of SQL 2005 to fail. You may have to uninstall the SQL 2008 first. Also take a look at: What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation to see if any of these suggestions helps. |
Last edited by: Michael K at: 10/6/2016 9:30:09 AMMichael |
|
Follow us on