10/7/2016 1:44 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
OK. So you mean in manual/JOG mode motor is running only in one direction. Assuming this true & refer the wiring diagram you attached in earlier post, it needs to be corrected. Pin 7 i.e. DI 3 is for CWL rotation & pin no 8 i.e. DI 4 is for CCWL rotation. So please correct the wiring. For more information, please refer attached sheets. AttachmentSINAMICS_V90_PIT control.pdf (446 Downloads) |
This contribution was helpful to
1 thankful Users |
10/7/2016 1:49 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, If you want to control V90 with S7-1200 PLC with HMI, please refer below FAQ which will give you detailed information.. SINAMICS V: Controlled Positioning of a V90 with S7‑1200 via the Pulse/Direction Interface, with HMI (Set 7) |
This contribution was helpful to
1 thankful Users |
Follow us on