7/23/2009 7:33 PM | |
Posts: 767 Rating:
|
Hi, Ideveloping a project with Step 7 and WinCC 7.0. It is a single user project (I started it as multi-user first but now it's single user as seen in attachment). I am testing it using PLCsim.I have created some messages using Alarm_DQ block which I can see in Alarm logging now after OS compilation. But my alarm control is keep complainingthat "All server connection failed" (see attachment). All my data is working the tags are updating but I don't know what server the alarm logging is looking for. By the way I am running this project on the ES or programmer but I have checked the option for allow activation on ES. AttachmentAlarmLoging.pdf (455 Downloads) |
7/23/2009 9:30 PM | |
Posts: 2661 Rating:
|
I cannot open the attachment... Regards |
7/24/2009 9:51 AM | |
Posts: 28 Rating:
|
same problem here with the attachment.... Did you activate "Alarm logging runtime" in the WinCC startup list? |
This contribution was helpful to
2 thankful Users |
7/24/2009 11:51 AM | |
Posts: 767 Rating:
|
Oh silly me... ye I did not... |
Follow us on