7/21/2025 12:49 PM | |
Joined: 2/1/2010 Last visit: 9/12/2025 Posts: 212 Rating:
|
Did you try to turn AcStart = 0 for several scans while GrErr is false? I don't have a live system to double check, and memory is not good enough, but I'm assuming you are comparing this against other drives and this is the only one with AcBusy = 1 all the time? Else it might just be indication that you've set AcRead = 1. EDIT: from PUD: So I think it's normal, but you can tell us if its only happening on 1 drive. Which specific Drive ES APL Library version? There are several hotfixes in the 9.x > 9.1 SP2 range that should be typically applied. |
Last edited by: RVS.wick at: 07/21/2025 13:01:49If my post helped you, please rate. Thanks. |
|
Follow us on