1/23/2012 4:19 PM | |
Posts: 63 Rating:
|
Salut, comment je peux charger dans mon PC un projet à partir de la pupitre sans carte mémoire? |
1/24/2012 9:23 PM | |
Posts: 63 Rating:
|
the panel is OP 177B mono DP color and a TP 177B |
1/25/2012 8:18 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, In order to take a backup of OP177B: 1. Software - Prosave (10347815)- (backup is not editable, only is possible to restore it in the same type of panel using Prosave software. 2. Software - WinCC FLex - Uploading only possible, if the Transfer of the current project file from the configuration computer to the operating unit must be performed using the Upload option "Enable backtransfer". Hardware: Connection cable between PC and panel - Projecttransfer_V1_2_e.pdf In order to take a backup from TP177B: 1&2 - thase am story as in case of OP177B. Hardware: Connection cable between PC and panel - Projecttransfer_V1_2_e.pdf Best regards, Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
Follow us on