1/16/2023 9:50 AM | |
Joined: 1/21/2013 Last visit: 9/6/2025 Posts: 4090 Rating:
|
Hi EntrepreneurAlvi,
for data exchange between two PLCs in different subnets, a SIMATIC PN/PN Coupler might be a good solution. When using IO data only, up to 1,440 bytes can be exchanged. A additional communication processor would allow the PLC to be connected to a additional subnet. So the PLC can be put into the subnet of the communication partner to enable "Layer 2" communication. Kind regards |
Follow us on