2/28/2022 6:16 PM | |
Posts: 257 Rating:
|
It could be the case that S7-1500 controllers are to communicate via the IEC 60870-5 protocols with telecontrol and substation control systems from different manufacturers. The necessary information is provided in the various FAQ articles: How can you implement the IEC 60870-5 protocols with the SIMATIC S7-1500? Software download / Trial - SIPLUS RIC V1.7 SIPLUS RIC - Delivery release SIPLUS RIC V1.7 SIPLUS RIC IEConS7 : Functional Description Version V1.6 Upd4 If the IEC 60870 protocols are to be implemented with the SIMATIC S7-1500, then an S7-1500 CPU and the SIPLUS RIC library with the corresponding SIMATIC S7 Memory Card are required. For example, the following configuration would be conceivable: SIMATIC S7-1500, CPU 1511-1 PN, central processing unit with working memory 150 KB for program and 1MByte for data, 1st interface: PROFINET IRT with 2 port switch, 60 NS bit performance, SIMATIC Memory Card required. Order. No. 6ES7511-1AK02-0AB0 plus SIPLUS RIC library for SIMATIC S7-1500/ET200SP consisting of SIMATIC SMC 12MB - CD (software, documentation) - Runtime licence Order. No. 6AG6003-8CF00-0LE0 Best regards, SIMATIC International Technical Support Hub |
Follow us on