3/12/2018 2:17 PM | |
Joined: 9/27/2006 Last visit: 9/14/2025 Posts: 12408 Rating:
|
Hello hamed; Please, every time you start a new thread, we would appreciate to know what hardware and software you are using. For example, what variant of PLCSim are you using, Simatic Manager or TIA Portal, and what version (v5.4, v14 SP1...). And which CPUs are you using in your project? Maybe these informations can help: http://w3.siemens.com/mcms/simatic-controller-software/en/step7/simatic-s7-plcsim/pages/default.aspx Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 3/12/2018 2:40:41 PM |
|
This contribution was helpful to
4 thankful Users |
3/12/2018 2:49 PM | |
Posts: 241 Rating:
|
hello i am using step7 v5.6 and plcsim v5.4 sp8 and this is my program Attachmentprofibus.zip (299 Downloads) |
Last edited by: hamed12580 at: 3/12/2018 2:58:36 PM |
|
3/12/2018 3:05 PM | |
Joined: 9/27/2006 Last visit: 9/14/2025 Posts: 12408 Rating:
|
Hello hamed; In that case the screenshot from the previous post should give you enough hints: build a single project with 2 different CPUs, each with its own hardware configuration and program. Download the complete project to PLCSim and start one instance for each CPU you want to simulate, including communications. The example below shows step-by-step how to open multiple CPUs simultaneously with PLCSim. https://support.industry.siemens.com/cs/ww/en/view/38726591 Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
3/12/2018 3:33 PM | |
Posts: 241 Rating:
|
hello i have read those steps and tried to connect cpus by profibus but i couldnt ,also i have attached my program and you can test it regards |
3/12/2018 3:55 PM | |
Joined: 9/27/2006 Last visit: 9/14/2025 Posts: 12408 Rating:
|
Hello hamed; You have not attached your program, and it would be up to you to determine what is wrong with your PLCSim configuration and correct it. You could start with the PLCSim manual for version 5.4 (which supports multiple instances) You can connect the 2 simulated CPUs over Profibus-DP, if you set the PG/PC interface to PLCSIM (Profibus). https://support.industry.siemens.com/cs/ww/en/view/54667828 Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
Follow us on