12/4/2023 6:10 AM | |
Joined: 12/16/2018 Last visit: 8/27/2025 Posts: 74 Rating:
|
I have installed Pcs7 V9.1 SP2 and need to adding Y-Link with 6ES7197-1LA12-0XA0 order number, Does any one know how to added this Y-Link? AttachmentAttachment.zip (466 Downloads) |
12/4/2023 6:46 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, I think this is because the MLFB you supplied is a Y link package. It consists of several items: Two IM153 modules, Y coupler and two bus modules (IM/IM and Y coupler bus). See attachment for details |
If I could help you, you can use the RATE button. Thank you. |
|
12/4/2023 12:46 PM | |
Joined: 12/16/2018 Last visit: 8/27/2025 Posts: 74 Rating:
|
Hi Oreca |
Last edited by: DPCS at: 12/04/2023 12:47:42Last edited by: DPCS at: 12/04/2023 12:48:23Last edited by: The Helping Hand at: 12/04/2023 14:24:12Link and text formatting optimized |
|
12/4/2023 2:42 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, Sometimes it's a bit of a challenge to find the information on the Siemens site. Try to use the following link to find information about components. You can search an item and sort by different criteria: I have found a very usefull document describing the Y link. Also it states what I already thought that you supplied a MLFB number that is a package consisting of several components. See the below link: |
Last edited by: Jen_Moderator at: 12/05/2023 05:39:57Link optimized. If I could help you, you can use the RATE button. Thank you. |
|
6/20/2024 9:42 AM | |
Joined: 8/8/2011 Last visit: 6/25/2025 Posts: 6 Rating:
|
@DPCS Did you get an answer for what part to configure the Y-link as in PCS 7? |
6/24/2024 3:48 PM | |
Joined: 11/10/2022 Last visit: 5/23/2025 Posts: 23 Rating:
|
Hi Dynamart, Attaching y-link as installed in the DCS panel. Also attached is the hardware configuration screen shot and form where you have to pull the y-link. Its quite simple, when put into network, you shall get a pop-up and have to define if the IM shall be as PA or DP. Trust this helps. Likewise, I have posted question (22/06/2024) on PCS7 (410E CPU) interface to drives and simocodes on profinet. In case you or anyone reading this post are aware, please help. Regards Nil Attachmenty-link.pdf (335 Downloads) |
Follow us on