11/8/2022 3:52 PM | |
Joined: 8/12/2021 Last visit: 8/20/2025 Posts: 351 Rating:
|
Hi guarri! It seems that you are creating a ring in your structure between the 2 Scalance and the program tells you that this is not possible. Why do you need to connect the two interfaces of the two Scalance? Maybe you can find some helpful information in the manual (17). It is possible that the option needs to be enabled.
AttachmentBA_SCALANCE-XC-200_76.pdf (780 Downloads) |
Last edited by: Jen_Moderator at: 11/09/2022 08:32:57PDF attached from link. If this Information really helps, you could use the Rate function |
|
11/9/2022 12:04 PM | |
Joined: 6/7/2022 Last visit: 11/10/2022 Posts: 4 Rating:
|
Hi Swarley92 I need to connect the two Scalance with optical fibers, because they must be redundant. Best reguards. |
Follow us on