1/9/2020 7:25 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, Yes, unfortunately you have to do this by hand. I hope Siemens will create a simple tool, like the IEA (Import Export Assistant) inside PCS7 (that comes with the PCS7 package) where you can do bulk engineering. PAA/COMOS is not created by Siemens, but an third party. In addition, if you have already created CM's with desired variants, you will notice you can copy them as well and then your variant has been set already, but I suggest you won't do this, because it is made clear in the manual that you must copy the CMT from master library to the plant hierarchy and not by copying the CM instances in the plant hierarchy, because connections can get lost when synchronizing the CMT. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on