3/19/2024 1:36 PM | |
Joined: 1/21/2013 Last visit: 9/10/2025 Posts: 4101 Rating:
|
Hi nilsig, As you can see in the list of supported alarm states, the acknowledgement is represented by bit number 2 (counting from 0). So you can use this to determine the state.
This includes alarms that do not need to be acknowledged. At this time, I do not know of any way to determine whether an alarm needs to be acknowledged or not. So the only solution I can suggest is to set the alarm filter so that only alarm classes with required acknowledgement are evaluated. Kind regards |
This contribution was helpful to
2 thankful Users |
Follow us on