4/13/2015 8:42 PM | |
Joined: 10/5/2014 Last visit: 8/12/2022 Posts: 243 Rating:
|
hello............., my question goes about an issue in the attached siemens tutorial. i excercised this tutorial in step 7 v5.5 and i learned a lot from it. But now i'am trying to do the same tutorial but than in tia 13. Everything went ok until i got to page 79- 80. I can not program the timer in a fc in my tia13 like they do in the tutorial. the timers are slightly different and i get db with it, and i don't get them in step 7 v5.5. and when i think that i'am finnished and i call the fc with timer in a ob (wich i have to do twice, page 80). the aren't working independently . please can anyone look at it and show me how to do the same like they do in the tutorial but than in tia 13 for the timer in the fc. gr gerard Attachmentaaab siemens working with step 7.pdf (723 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on