10/21/2010 8:34 AM | |
Posts: 1 Rating:
|
hi This is swapnil, can ne 1 provide me download links for Siemens PCS7 V6.1 Sp4 and also recommend me which antivirus i should install in my ES/OS for complete protection.
Splitted from Delivery release of PCS7 V6.1 SP4. |
Last edited by: O_Moderator at: 10/21/2010 10:57 AMnew subject after splitting |
|
10/21/2010 11:09 AM | |
Posts: 378 Rating:
|
Hello, as i understand it from the following entry, you have to order it if you don´t have a "valid Software Update Service agreement". SIMATIC PCS7 v6.1 + SP4 Released for Delivery About the Antivirus i think you should take a compatible software which can be found in following entry With what are SIMATIC PCS 7 V7.x, V 6.x, V5.x and V4.x compatible? Best regards Bilao |
Follow us on