2/24/2022 3:22 PM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello If you do so, then you also have to use Ethernet in the Transfer Settings in the Panel!! you cannot change it only on one side. Check also if the other tips do not work if you have deactivated the option validate Signatures in the Panel´s Transfer settings. Check also if your Engineering PC has a fixed IP in the same subnet as the Panel as. And if you cannot get it work you can also work with plan B: https://support.industry.siemens.com/cs/de/en/view/109740696 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on