7/20/2017 10:23 AM | |
Posts: 6 Rating:
|
Dear All, I am facing same problem (error a021 and a022) in Simoreg drive 6RA7018 - 6DB6262 - 0 - Z when ever i try to reload the parameter.All the drives are connected via Profibus with PLC s7-300. Even i tried to program by disconnecting all the connections but still i am facing same error. But when i tried with same CUD1 card in another unit i was success full but i am not able to do so with same electronics box. Please guide me to resolve the issue. Parameters are as below mentioned :- P360 - 1- 0 P360 - 2 - 0 P360 - 3 - 0 P360 - 4 - 0 P675 - 1 - 1 P675 - 2 - 1 P686 - 1 - 1 P688 - 2 - 1 P689 - 1 - 1 P689 - 2 - 1 Regards CB SINGH ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/27/2017 8:38:41 AMNew subject after splitting |
|
7/20/2017 11:27 AM | |
Joined: 8/25/2006 Last visit: 6/27/2024 Posts: 2207 Rating:
|
Hello. What is the value in P649? If P649<>9 then P688 and P689 are not effective. |
7/22/2017 11:09 AM | |
Posts: 6 Rating:
|
The value of P 649 is 3002. |
7/26/2017 11:48 AM | |
Posts: 6 Rating:
|
Hi i tried this way also and got " download for file DS1 successfully completed " But i am getting A021 and A022 on my drive bop |
9/21/2022 4:08 AM | |
Joined: 9/20/2022 Last visit: 9/21/2022 Posts: 1 Rating:
|
How was this issue resolved |
Follow us on