3/26/2021 3:41 PM | |
Posts: 198 Rating:
|
Hello, With respect to failsafe acknowledgement, apart from the user authorizations, it is a transaction which can only be performed by an individual operator who initiates, checks, and confirms the change. However, one transaction can be performed by two operators. The first operator initiates the change (initiator) and the second re-enters, checks, and confirms the value (confirmer). Operator authorizations are set in the faceplate properties. The connection IDs are generated by the system automatically, in contrast with SDW. A detailed explanation about the SWC_QOS allied concept of 'Failsafe acknowledgement' is found the Process Safety Manual (Section 7.10.1) in the link below: Process Safety Manual - Compendium B Hope this helps |
Last edited by: Jen_Moderator at: 03/29/2021 10:27:59Optimized link. |
|
8/27/2024 5:23 PM | |
Joined: 1/8/2024 Last visit: 8/2/2025 Posts: 12 Rating:
|
Hello, Did you figure out how the acknowledgement works? I have the same problem |
Follow us on