8/19/2025 11:10 PM | |
Joined: 3/28/2010 Last visit: 9/4/2025 Posts: 1171 Rating:
|
The 7ME6520 is the 5100W flow tube, designed for potable water service. In the part number 2nd 5 digit field, the code 2 is for EPDM and the code 3 is for NBR hard rubber. The Siemens materials compatability guide is attached. Sodium Hypochlorite is listed as 'moderate' resistance for pure solutions at 20 Deg C. One would assume that a flow tube designed for potable water would tolerate disinfection with a chlorine solution, given that ubiquitous presence of chlorine in water treatment. AttachmentSiemens Chemical Resistance Chart magmeter.pdf (99 Downloads) |
Follow us on