6/25/2014 9:06 AM | |
Posts: 49 Rating:
|
Hello gents, Can anybody help on this topic?? please respond even if you have slightest clue on the topic. Regards, Enigma
|
6/25/2014 9:54 AM | |
Joined: 10/7/2005 Last visit: 9/8/2025 Posts: 3049 Rating:
|
Hello Enigma you can certainly read out the Diagnostic data of Y-Link underlying DP Slaves as well as determine "simple" things like whichof the underlying DP Slaves has faulted completely, has a module fault, is ok etc. The "trick" is that all this data is read out from the Y-Link's ET200M's itself instead of directly from each underlying DP Slave (The Y-Link is oneDP Slave to the H Systems and forms a new DP Master system for the underlying DP Slaves). Have a look at chapter 13.2 of the SIMATIC Bus links DP/PA coupler, active field distributors, DP/PA Link and Y Link which contains the details of the data records and SFC's to use and note especially the SFC13 example in chapter 13.2.4.2. I hope this helps |
Cheers |
|
Follow us on