6/28/2025 10:37 AM | |
Joined: 1/29/2019 Last visit: 8/18/2025 Posts: 27 Rating:
|
Hello everyone, I am currently commissioning a servo drive using the SINAMICS Control Unit CU320-2 DP (6SL3040-1MA00-0Axx, Firmware V5.2.3) via PROFIBUS. The connection through SINA_POS is working correctly — the drive is under control, and basic communication is established. However, I am facing issues with reading drive and motor parameters using the Free Telegram interface. I have added the Free Telegram configuration and assigned it to parameters I want to monitor — for example, motor temperature (r0035). The PLC is receiving data from the drive, but the values do not make sense and appear unformatted. 🔹 My questions are:
Thank you in advance for any help or documentation references you can share. I'm trying to properly monitor motor status and send control values via Free Telegram but struggling with the data format and interpretation. Best regards, AttachmentAttachment.pdf (125 Downloads) |
Last edited by: Ami39 at: 06/28/2025 10:52:05 |
|
Follow us on