7/10/2010 12:42 AM | |
Posts: 7 Rating:
|
I have not completed reading through the chapter yet, but I have a question also. I have received the message informing me to INITIALIZE the device. My siprotec relay (7SJ64) is in operation and has been for years. I now need to connect, but if I understand this INITIALIZE procedure, I will be overwriting the data on the relay with the data on the PC? I do not believe I have a copy of the "exact" file that was downloaded to the relay in the past. How do I now connect and "upload (relay -> pc)" the configuration (without taking the device out of operation)? (This is a 24x7 operation and I cannot "stop" the process). Thanks in advance. Back to reading in hopes I find the answer quickly. Genglish Splitted from Digsi interface port. |
Last edited by: O_Moderator at: 7/12/2010 12:32 PMLast edited by: O_Moderator at: 7/12/2010 12:31 PMnew subject after splitting |
|
9/11/2013 7:58 AM | |
Posts: 1 Rating:
|
did u find a solution to your answer..? because am facing the same problem.. |
Follow us on