9/27/2017 10:04 PM | |
Joined: 10/7/2016 Last visit: 5/22/2024 Posts: 66 Rating:
|
Hi all, Someone can explain me how FB110 works? Or some manual that explain it. My CPU is 928B |
9/27/2017 10:23 PM | |
Joined: 9/27/2006 Last visit: 9/16/2025 Posts: 12409 Rating:
|
Hello Gustavo; If you mean FB 110 "MSGOUT", look at section 10.9.2 of the following mnual: S5-135U CPU 928B Programming Guide - Industry Support SiemensFB 110: Transferring a data block Task The data area to be transferred is stipulated by the input parameter FIRB (= number of the first data field to be transferred) and NUMB (= number of data fields to be transferred). A data field normally consists of 32 data words. Depending on the data block length, the last data field may be less than 32 data words. The transfer is triggered by a positive-going edge at the start input STAR. If the output parameter REST is zero after the transfer, this means that the function block TRANDAT was able to send all the data fields (according to the NUMB parameter)... Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 9/27/2017 10:24:19 PM |
|
9/28/2017 1:24 PM | |
Joined: 10/7/2016 Last visit: 5/22/2024 Posts: 66 Rating:
|
No, is this one in attachment |
9/28/2017 1:53 PM | |
Joined: 7/18/2011 Last visit: 4/11/2025 Posts: 521 Rating:
|
Hello, Check FB114 p5.38 Kind regards, BV AttachmentS5_Modulare_PID_und_Fuzzy-Regelung_e_OCR.zip (391 Downloads) |
9/28/2017 1:56 PM | |
Joined: 12/18/2014 Last visit: 9/17/2025 Posts: 35967 Rating:
|
No, it's not the same. The user Gustavo Dias refers to a selfmade function block from the programmer of an S5 project, which the user wants to translate to S7. In attachment the FB. AttachmentFB110.pdf (437 Downloads) |
9/28/2017 9:55 PM | |
Joined: 10/7/2016 Last visit: 5/22/2024 Posts: 66 Rating:
|
Sorry guys, this FB110 is not a default block is a self block. |
Follow us on