6/24/2024 8:32 PM | |
Joined: 6/11/2021 Last visit: 9/2/2025 Posts: 2 Rating:
|
hi friends I have two PLCs from two different projects and each plc has a different subnet when I try to communicate between them by PUT/GET or TCP communication the software tells me that I need to use a router because I have two different subnets I tried with some different routers but I could not fix them although I can reach the PLCs by ping test Does the function need a specific router or special parameters I was wondering if there was a proper solution for this application, without a PN/PN coupler. I was looking for smaller solutions to utilize two different subnets within the same network infrastructure. In my case, I have two different projects (TIA), each one has a 1515F CPU with remote F-DI/Os (up to 680) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/25/2024 05:21:00New subject after splitting. Text formatting optimized. |
|
Follow us on