3/30/2019 7:40 PM | |
Joined: 1/30/2018 Last visit: 10/16/2022 Posts: 12 Rating:
|
I almost follow what you are doing here, but I have a slightly different issue. I have a pressure-based tank level sensor that has a range of 0-10 meters. If I have a tank that is only 6m tall, I want the reading at 6m to register on the display as 100% full. So when I set up an amplifier for 4...20 mA, do I keep Min to 0, change Max to 600 and let the gain and offset fields correct by themselves? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/1/2019 7:48:46 AMNew subject after splitting |
|
Follow us on