9/27/2022 8:44 PM | |
Joined: 3/30/2014 Last visit: 8/5/2025 Posts: 88 Rating:
|
Good. My LOGO! project does what it's supposed to do. Now I come to the next challenge. HMI KTP700 Basic (2GB03). I have already been able to fill in the VM mapping with regard to "control". I have to use version 15. But now I want to integrate "rolluiken" (shutters, blinders) into the HMI. The TDE could then disappear. If I'm right, I can use the buttons on the HMI. Instead of the TDE. And now I'm stuck somewhere. Who wants to put me on the right track? ------------------------------------------------------------------------------------------ AttachmentHoefsmid 21_V2.zip (842 Downloads) |
Last edited by: Jen_Moderator at: 09/28/2022 03:39:51New subject after splitting |
|
9/28/2022 2:14 AM | |
Joined: 12/18/2014 Last visit: 9/12/2025 Posts: 35955 Rating:
|
If you have created a HMI project then upload it. |
9/28/2022 4:35 AM | |
Joined: 3/30/2014 Last visit: 8/5/2025 Posts: 88 Rating:
|
Sorry, forgot to type 15.1 in my haste. The project I have now uploaded is far from finished. But then you already have an idea of what it will look like. For me the "blinders" can also be in the root screen, at least if there is room for them. [snip]
AttachmentProject5.zip (593 Downloads) |
Last edited by: Jen_Moderator at: 09/28/2022 05:05:38Division of questions into separate topics. |
|
Follow us on