7/24/2024 4:34 AM | |
Joined: 11/21/2020 Last visit: 8/26/2025 Posts: 213 Rating:
|
Hi, In this video ( https://www.youtube.com/watch?v=e2ptCp2QnbM&ab_channel=GeneralTechnologyKnowledge ) a guy uses S7-1200 PLC and Beckhoff 05.2420.1230.1024.5009 HTL encoder to measure motor RPM. I am using instead of Beckoff Pepperl's HTL encoder 10-11651_R-1200 (datasheet is in the pdf attached). The problem is that in his case counter resets to 0 after he stops to rotate the encoder's shaft. In my case it is not resetting, it continues to increase.Is it realted to my encoder, or with settings/program? My encoder's power supply is up to 30V, but for some reason it is getting real hot after I connect it to PLC (I use for encoder's supply L+ 1 and M+M1 shorted). What could be the problem? Is the formula in his video correct Speed (rpm)=[Value of Encoder (frequency) / Encoder Resolution] *60 AttachmentBinder1.pdf (520 Downloads) |
Last edited by: milos23 at: 07/24/2024 04:35:15Last edited by: milos23 at: 07/24/2024 07:04:48Last edited by: Wit_Moderator at: 07/25/2024 10:55:54Video embedded |
|
Follow us on