11/12/2014 3:06 PM | |
Posts: 9 Rating:
|
Hi all, When you are inthe diagnostic overview,you can see all information about (for example) a missing module. Also the short name and the order number is shown. Now I would like to show an alarm automatically when a module is missing or broken. This works perfectly. But when I push the tooltip (help-button) the short name and the order number are not shown correctly. Only the address where the order number and short name should be are shown. Why is it finding this correct information with the diagnostic overview and not with the alarms? By the way, I am using IM-151-8 CPU and KP400 Comfort. AttachmentC:\diagnostic.pdf (269 Downloads) |
Last edited by: doedel at: 11/12/2014 9:09 PMLast edited by: doedel at: 11/12/2014 4:47 PMLast edited by: doedel at: 11/12/2014 4:45 PM |
|
Follow us on