6/30/2021 6:19 PM | |
Joined: 10/9/2020 Last visit: 8/28/2023 Posts: 9 Rating:
|
Hola Hay una manera de reseteo de fabrica de un iot 2040? o la manera de saber con que ip esta trabajando actualmente? Quiero obtener su ip de fabrica que es la 192.168.200.1 Ya que tubo un uso y no se la ip con la que estaba trabajando. Espero su ayuda.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/01/2021 09:05:26New subject after splitting |
|
7/1/2021 12:07 AM | |
Joined: 12/12/2016 Last visit: 7/25/2025 Posts: 640 Rating:
|
Hello, If you don't have the IP of your IOT anymore you can check with wireshark if you can identify the source of any packets coming from any of the interfaces of the IOT. Alternatively you could connect it with a router and hope one of the interfaces is still set to dhcp. Or you could also connect an FTDI cable and login with putty using UART communication. If you want setup the IOT from scratch you can follow the Setting Up guide once again to reflash the image onto the SD card. Best Regards! |
Follow us on