9/4/2020 6:14 AM | |
Joined: 2/4/2015 Last visit: 7/1/2025 Posts: 72 Rating:
|
Dear all, We have S120 drive for chute rotation application with servo motor. Earlier it was running with resolver. Now we have bypassed resolver as there is issue with resolver in motor. Now we are facing over speed fault intermittently. Maximum speed is 2000rpm, p2162(hysteresis) is 40rpm. Speed setpoint is 1174rpm. In encoderless speed is calculated based on current. Should i repeated motor ID run?? Surendhar M ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/04/2020 09:37:42New subject after splitting |
|
Follow us on