4/29/2025 6:24 PM | |
Joined: 2/12/2025 Last visit: 9/9/2025 Posts: 7 Rating:
|
Hello everyone, First of all thank you for reading my post! Currently I'm having a view small problems with my mp377 panel. I'm trying to load a new program into it, but I'm only getting strange errors. When I try to connect to the device I can see it's name, I can change it, and I can flash it's LED. But as soon as I try to load to the HMI panel the loading takes super long and I eventually get a error code that the device cannot be reached. The second strange thing I had that the program did compile but I got the message: "Incorrect version of operating system is installed on the device" I have never seen this error before I also can "factory" reset the device but then only the device name and it's IP are lost for a small moment. I am not able to delete the entire program. Is there anyone that maybe knows these faults, and who has a solution for them? I'm looking forward to your replies! Kind regards, Jobbbooo AttachmentMP377 faults.pdf (196 Downloads) |
4/30/2025 8:52 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Please have a look at the following link: Why can you not transfer the HMI configuration to the panel? And it looks like there is a wrong image installed on the HMI. Here a link how to perform an OS update: Best regards, Wizard |
Follow us on