9/19/2021 9:48 PM | |
Joined: 8/6/2019 Last visit: 9/11/2022 Posts: 2 Rating:
|
Someone has managed to communicate Logo! with a Variable frequency drive? Will you have an example?
|
9/20/2021 5:41 AM | |
Joined: 12/18/2014 Last visit: 9/7/2025 Posts: 35933 Rating:
|
Hello williamzc, all LOGO!s 0BA8 can Ethernet TCP/IP with the S7 protocol. Since the LOGO!8.1 they can also Modbus TCP/IP. You don't write which type of communication you want to use. I think you want Modbus TCP/IP because you post also in this topic: Can the LOGO! Modbus TCP?And please don't post twice for the same problem. |
Follow us on