10/6/2010 12:01 AM | |
Posts: 5 Rating:
|
hello fux, i analysed your speed control. But i want to change speed only one button.For example when i push button,motor speed will be %20 nad then push the same button speed will be %40 and then %60, %80,%100 at the end whan i push the button motor stop. and then i push button, motor speed again %20,%40,60%, 80%, 100%... İ will be glad, for your hepl. Splitted from Logo speed control. |
Last edited by: O_Moderator at: 10/6/2010 1:21 PMnew subject after splitting |
|
10/8/2010 2:05 PM | |
Posts: 2930 Rating:
|
Hi, check this example: Hope this helps AttachmentOne Buton control analog.zip (571 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on