6/23/2016 2:13 PM | |
Posts: 11 Rating:
|
So setting input to 4 to 20mA just removes the bottom 200 count giving the resolution a max 800? |
6/23/2016 5:57 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35964 Rating:
|
Yes, that is correct. |
6/29/2016 2:34 AM | |
Posts: 11 Rating:
|
i have written the software that accumulates 100 samples, totals, stores and displays them, clears the accumulator and starts again On an 0bA6 runs perfect in simulation showing 15 bits (0 to 32700 or 16bits using -32700 to +32700) changed it slightly adding only 30 samples and display divided by 3 to display 100.00 changing (B4 to 100) and (B5 V2 to 1) will restore to previous state but will not read inputs above 3.2V without error
Attachment10to15bits.pdf (462 Downloads) |
Last edited by: Total Madness at: 6/29/2016 3:20:06 AMLast edited by: Total Madness at: 6/29/2016 3:45:15 AM |
|
Follow us on