12/8/2021 12:36 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Hello, Please refer below links, may be helpful to you. |
12/9/2021 5:14 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Hello, 6RA24 & 6RA80 DC drive technology is different. For 6RA24 drive monitor is toool which user dan use to upload & download parameters with little bit help to go on line. Tacho/max speeed. field current setting is manual. For 6RA80 - is latest technology wherein all motor related parameters can be set & no manual adjustment is required. Starter - free download is tool with which user can go on line, upload & download parameters, plus use tracing for fault analysis, DCC charts, free function blocks etc. etc feature are available. Also 6RA80 has standard BOP for parameter setting & visualisation as well memory card option is available to store drive parameters & for parallel drive commissioning. 6RA80 drives can be used as master-slave, standard standalone, connected in network & communication can be established. More details you can find in Catalog D 23.1 - SINAMICS DCM DC Converter, Control Module. |
This contribution was helpful to1 thankful Users |
Follow us on