1/22/2015 2:07 PM | |
Posts: 510 Rating:
|
Mr. programmer, The error message indicates WinCC Flexible is not installed on the computer with TIA Portal installed and you did not use the Migration tool on the WinCC flexible project as an intermediate step. Alternatively, using the “Migration Tool”, you can convert the source project into the migratable “*.ap12” file format. This file can be imported through the TIA Portal. Then you will not need STEP 7 V5.x (WinCC Flexible 2008 SP2 or SP3) on the PC. Notes • For WinCC V12 or higher you will find the migration tool on the installation DVD under the “Support → Migration_Tool_TIA_V12.exe” folder. The following link contains a Migration manual that you may find very helpful: http://support.automation.siemens.com/WW/view/en/77430539 Good luck, billwest |
Follow us on