1/28/2016 12:18 PM | |
Joined: 8/25/2014 Last visit: 8/17/2025 Posts: 172 Rating:
|
Motor not burn due to drive or overcurrent. One electric fan burned near the motor and it effected the motor. |
4/20/2016 1:18 PM | |
Joined: 10/10/2010 Last visit: 7/5/2025 Posts: 309 Rating:
|
motor data identification is more perferable at this case during vector control |
4/27/2016 10:31 PM | |
Posts: 198 Rating:
|
first configure accurately motor parameters each and every thing required in parameters then see operation manual then select auto tone function select yes then your drive automatically analyze your motors parameters and your set parameters if these parameters matching with drive system parameters then drive will tell auto tune test pass otherwise fail. Hope this will help During auto tuning motor behavior see in video |
This contribution was helpful to
1 thankful Users |
Follow us on