11/13/2024 10:34 AM | |
Joined: 8/10/2021 Last visit: 5/6/2025 Posts: 14 Rating:
|
Good morning, everyone. We have a power module 6SL3120-1TE23-0AA3 (30A) that controls 13 motors rated at 0.45 kW (1.3 A) each (wiring diagram attached). We have occasionally experienced motor burnout, and upon checking, we found that the no-load current for each motor is 2.4 A (which is 184% of the rated no-load current). We checked the electrical connections, and everything appears to be in order, so I suspect there may be an issue with the power module settings (parameterization). I would appreciate any assistance in resolving this issue. Thank you. Attachmentwiring diagram.pdf (157 Downloads) |
Follow us on