6/25/2021 9:22 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, OK, because it looked to me that the FbDrive is getting feedback that the drive is running, but in fact isn't, maybe that's why the error came. In the template (Drive) the On signal is connected to Fwd or Rev control signal from the MotSpdCL. It could be something with the hardware configuration (incompatible Profidrive telegram, incorrect GSD/GSDML, are the driver connections like PZDIn2,3, etc created automatically? |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
6/25/2021 11:13 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, Yes we had trouble with the Fbdrive as well handling only two telegrams. Also only Profidrive telegrams can be handled. For our application we used PPO types (Danfoss) and therefore created a custom block in SCL to handle the communication (Read in data from status word, send data to control word etc.) |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
7/2/2021 11:02 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, See the following link for more info: |
If I could help you, you can use the RATE button. Thank you. |
|
7/2/2021 11:13 AM | |
Joined: 4/28/2015 Last visit: 4/17/2025 Posts: 37 Rating:
|
There is no answer |
Follow us on