11/22/2024 9:10 AM | |
Joined: 11/10/2022 Last visit: 5/23/2025 Posts: 23 Rating:
|
Hello Everyone, Greetings. Have been working on PCS7 (410H) and ET200 SP HA IO System. Following are my doubts and need some help/advice to understand:
Regards Nil AttachmentNew Microsoft Word Document.docx (120 Downloads) |
11/22/2024 11:31 AM | |
Joined: 3/14/2008 Last visit: 9/8/2025 Posts: 2216 Rating:
|
Hi, Those bits for input/output are so called quality bits. They are generated from the module to indicate the signal is good. You can name them, but it's not required. The signals are connected automatically when generating the module drivers. |
Last edited by: Oreca at: 11/22/2024 11:35:47If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on