6/28/2025 6:22 AM | |
Joined: 11/17/2023 Last visit: 9/12/2025 Posts: 1 Rating:
|
HI, PLC going to STOP mode and it starts if i restart by using Manual Reset, Again after 2 or 3 hrs again it is going to STOP Mode. As per Diagnostic Buffer it shows below mentioned error, CPU MODEL:6ES7412-5HK06-0AB0 Event 15 of 120: Event ID 16# 457F STOP caused by STOP command Breakpoint in user program: Cyclic interrupt OB (OB 35) Priority class: 12 FB number: 49 Module address: 10694 Previous operating mode: RUN Requested operating mode: STOP (internal) Event occurred in the master CPU in rack 0 Internal error, Incoming event 12:46:16.414 PM 06/27/2025 (Coding: 16# 457F F884 8E70 0C23 0031 29C6) Entire Diagnostics copy attached Kindly reply with solution. AttachmentDiagnose27jun.txt (108 Downloads) |
Follow us on