4/3/2025 9:48 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello Drago1305 in WinCC V7/8 only 64 Connections for S7300/400 are supported: https://support.industry.siemens.com/cs/ww/en/view/109976749/183762275851 And you would need a full additionally Softnet S7 License for more than 8 connections. You should check if it makes sense to use one or more extra PLCs that do the communicatino with a few PLCs to collect the information in order to reduce the PLC connection number. Also you could use some other ways in the middle like an OPC UA Server or similar Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on