5/21/2015 1:21 PM | |
Posts: 2 Rating:
|
Hello. When we change the output to 50% we measure 15mA (69%), and when we manually send 100% we measure 20mA. Basically our problem is that the actual analog output doesn't match up with the PID-output on TIA-portal. This problem occured on both modules. In attachment are some screenshots from our program, and wiring diagram.
Thanks AttachmentScreenshots.zip (234 Downloads) |
Last edited by: Henriksj at: 5/21/2015 1:24:51 PMLast edited by: Min_Moderator at: 5/22/2015 10:30:45 AMMove pictures in attachment |
|
5/26/2015 9:17 AM | |
Posts: 2 Rating:
|
Which values do you recommend on the scale_x block? |
Follow us on