9/27/2012 4:56 AM | |
Posts: 113 Rating:
|
what are the security methods available in s7 cpu to avaoid changing a running program |
9/27/2012 5:27 AM | |
Posts: 1064 Rating:
|
If your plc is capable password protect for read write or know how protect if you do not want them to see the program |
9/27/2012 7:58 AM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
hello, Have a look at: How can you activate the protection level with a password in the HW Config for an S7 CPU? Regards, Marcjan |
Problem solved? |
|
9/28/2012 3:11 AM | |
Posts: 113 Rating:
|
The same i did,but supose the put a new cpu instead of the current cpu...and installing my running program .how can i stop the machine in a not working state. |
9/28/2012 7:23 AM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, If customer allready has the program there is not mutch you can do that stay friends and give good service, then he will call you if in trouble. If you are afraid he sells your program, sorry it's too late. There is way to make it run only on this mmc and CPU. Read out the serial numbers with SFC51, do a compare if not o.k. you dont run the progam. How can you read out the identification data (the serial number of the MMC, for example) with the SFC 51 in STEP 7 V5.5? But in your case it's to late for that. Regards, Marcjan |
Problem solved? |
|
10/2/2012 11:26 AM | |
Posts: 51 Rating:
|
Thanks for your post |
Follow us on