11/2/2017 8:54 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi PMVisser, Recipes are a functionality of WinCC Recipes are stored in the Panel and can be loaded to the PLC. Have a look to the following application sample: Creating a Standard Recipe View and Recipe Screen with WinCC (TIA Portal) hope this helps, regards, |
FCK WAR! |
|
11/3/2017 3:26 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating:
|
See if this works for you. AttachmentMultiplexing_Example.zip (1105 Downloads) |
11/3/2017 10:50 AM | |
Joined: 5/20/2014 Last visit: 9/26/2022 Posts: 57 Rating:
|
Right under where you set the acquisition mode you also set Acquisition cycle, which by default is 1s. If you use 2Hz for your trigger then the trigger bit will always se the same state (therefore there will be no value change for the event), see here for more details: http://tiaportalhowto.com/en/blog/tia-portal-clock-memory/ As Wizard advised don't use clock bits. Instead use your program sequence logic to trigger the record loading, when you need it. Use rising edge + extended pulse combination (longer then 1 second ;) ) just to be 100% sure the HMI will read it. For the purpose of testing just use memory bit and toggle the state (ctrl + F2, ctrl + F3)
|
tiaportalhowto.com -> TIA Portal Tips, Tutorials, Videos, and more... |
|
11/3/2017 11:31 AM | |
Posts: 32 Rating:
|
Hello Robert and Wizard, Thank you for your reaction. But I tried both of your solutions but it also didn’t work. As you can see the RecipeNo is 1 and the RecipeDataNo is 2. I don’t know if it is important information but when I open the “recipe screen” and when change one of my data record. When I change the Data Record Name it opens it and almost instantly goes back to an empty data record.
|
11/3/2017 11:58 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello PMVisser, Is it possible to share your project with us? Best regards, Wizard |
11/3/2017 12:09 PM | |
Posts: 32 Rating:
|
Hello, Sorry, it’s not in the 3000 kB range of the forms. |
Follow us on